Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the HOM2150BB, HOM2175BB, HOM2200BB, and HOML2225 be used in CSEDs?
Issue:
Application

Product Line:
CSED

Resolution:
These larger branch breakers can ONLY be used in the CSED that shows them listed on the wiring diagram of the device.

The specific devices will be marked for a branch breaker of 200 A max. So these high amp branch breakers (HOM2150BB, HOM2175BB, and HOM2200BB) can be used in those specific CSEDs that are rated 150 A or higher.
These larger branch breakers will require 4 pole spaces for mounting.
Also, the subfeed lug kit (HOML2225) could be used on the same devices, BUT the wiring diagrams will ONLY show a 200 A maximum branch breaker, so a local code inspector may not allow the use of the subfeed lug kit because it is rated at 225 A.

NOTE: The branch circuit breaker or subfeed lug kit ampacity cannot exceed the CSED mains ampacity rating.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings