Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a QO2150, QO2175, QO2200, or QO2225SL be used in the CSED all-In-one and meter main devices?
Issue:
Product Design Feature

Product Line:
Combination Service Entrance Devices

Resolution:
These high amp branch breakers and subfeed lug kit can be used in the appropriate CSED devices. See either the wiring diagram of the device or the drawing for each specific catalog number for the maximum branch breaker ampacity allowed.

NOTE: The branch circuit breaker ampacity cannot exceed the CSED mains ampacity rating.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings