Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What material is used in the construction of back boxes of Square D`s Hospital Isolated Power Systems and associated accessories?
Issue:
Back box material for Hospital Isolated Power Systems.

Product Line:
Isolated Power Panelboards.

Environment:
Product Characteristics.

Resolution:
The back boxes are made of 14 gauge steel degreased phosphatedand finished in baked gray enamel. The only exceptions are the Duplex Isolation Panel and Surgical Facility Panel which utilize 12 gauge steel.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings