Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the NEMA rating of busway plug in units?
Issue:
Nema rating of Busway Plug-in.

Product Line:
Busway

Environment:
I-Line Busway Plug-in units

Resolution:
Per UL857, the Busway Plug-in units are not NEMA rated. They are only rated as indoor devices.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings