Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can an EZM main terminal box be converted to either a main breaker or main fusible switch device?
Issue:
Product Design Features

Product Line:
EZM Metering equipment

Resolution:
No, The EZM main lug terminal boxes CANNOT be converted to a main breaker or main fusible switch. The physical components are not available inside the terminal box and cannot be field installed. Also, this would VOID the UL listing and violate the NEC, because it would change the device catalog number.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings