Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can an NQOD panel with a back-fed QO(B) main breaker be converted from top to bottom feed and vice versa?
Issue:
NQOD panel with a back-fed QO(B) main breaker converted from top to bottom feed and vice versa

Product Line:
NQOD Panelboards.

Environment:
Installation.

Resolution:
Yes. Rotate the interior 180 degrees.

NOTE: On NQOD panels with back-fed integral main breakers, the location of the main breaker will change when the panel is rotated. The standard M/B location on a bottom feel panel is bottom left. When the panel is rotated for top feed, the new main breaker location is top right.


CTA-ID : 2007621

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings