Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a 400A subfeed breaker, be added to a NF panel in the field?
Issue:
Installation of a subfeed breaker on a NF panel.

Product Line:
Panelboard

Environment:
NF panel

Resolution:
A 400A subfeed breaker can be added to 600A and 800A interiors only and it is only available as factory assembled. This can be selected in the product selector tools.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings