Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are any of the Square D safety switches plenum rated?
Issue:
Product Design Features

Product Line:
Heavy Duty, General Duty, and Double Throw Safety Switches

Resolution:
There are no plenum rated safety switches or applications for the use of a safety switch in a plenum area. The NEC addresses these types of application and installation of products. The local jurisdiction having authority would need to address this application.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings