Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are EZM metering branch devices provided with the tenant breakers factory installed?
Issue:
Does Square D provide factory installed tenant breakers on EZ Metering branch devices?

Product Line:
Metering Equipments

Resolution:
The tenant breakers must be ordered separately for 125 and 225 A devices. The tenant breakers for all the 400 A meter socket EZM branch devices are factory installed as standard.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings