Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the the aluminum wire lugs for a 9422TF2?
Issue:
Wire Lugs replacement for 9422TF2 Disconnect Switch.

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
9422 Flange Mounted Disconnect switches

Resolution:
Use part number 25065-04501 (quantity of 6 required) for the standard aluminum lug. For the optional copper lug, use part number 25050-34404 (quantity of 6 required).

NOTE: The standard aluminum lug is now obsolete

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings