Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the MP Meter-Pak devices available with a overall main breaker?
Issue:
Product design

Product Line:
MP Meter Pak

Environment:
Device Mains

Cause:
Application

Resoution:

No, The MP Meter-Pak devices are ONLY available as Main Lugs devices. There is NO overall Main Breaker or Switch available. If an overall main breaker or switch is required or preferred, look at the EZM Metering product line.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings