Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are Homeline load centers available in a NEMA 4, 6P, 8, 7, 9, 10, 12, or 13 enclosure?
Product Line:
Homeline Load Centers

Resolution:
Homeline load centers are only available in NEMA 1 or 3R enclosures. For other applications, consider using a panelboard.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings