Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
I received a replacement control station plate for my Model 6 LVMCC unit, but the latch on the control station plate does not line up with the latch pin. Is this the correct control station plate?
Issue:
Control station plate for Model 6 LVMCC

Product Line:
Low Voltage MCC

Environment:
Maintenance

Resolution:
Yes, in May 2000 there was a manufacturing change to the Model 6 control station plate.  The new control station plate can be used on pre-May 2000 Model 6 units by using the Control Station Plate Latch Pin Retrofit Kit, part number 80420-893-50.  See the document link for the installation instruction bulletin on the retrofit kit.



CTA-ID : 2007824

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings