Issue:
Current design repair parts
Product line;
QMJ Branch Switches
Resolution:
This QMJ device is only a single switch and it cannot be modified in the field to add an additional switch. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly - 4051239950 (1 required)
Load Base Assembly - 4052107750 (1 required; includes lugs)
Handle Knob Kit - 4028343750
Lug Assembly - 4025101851
Lug mounting screw - 2192620320
load base mounting screw - 4020506501
Current design repair parts
Product line;
QMJ Branch Switches
Resolution:
This QMJ device is only a single switch and it cannot be modified in the field to add an additional switch. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly - 4051239950 (1 required)
Load Base Assembly - 4052107750 (1 required; includes lugs)
Handle Knob Kit - 4028343750
Lug Assembly - 4025101851
Lug mounting screw - 2192620320
load base mounting screw - 4020506501
Released for: Schneider Electric USA