Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the coil burden of the shunt trip for the EDB, EGB, and EJB breakers?
Issue:
What is the coil burden of the shunt trip used for E-frame breakers?

Product Line:
E-Frame Circuit Breakers

Resolution:
The maximum coil burden is 288 VA. A 50 VA supply transformer is recommended.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings