Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How does a Q1-150AN neutral lug mount on an NQOD neutral assembly or ground bar?
Issue:
How to mount a Q1-150AN neutral lug on an NQOD neutral assembly or ground bar.

Product Line:
NQOD panelboards

Environment:
Installation/Setup

Resolution:

For mounting on neutral bar assembly:

1. Remove three adjacent wire binding screws from neutral bar.
2. Mount connector plate to neutral bar using two 1/4-28 screws. Torque screws to 35 IN lbs.
3. Mount neutral branch lug on connector plate with #12-24 pan head screw. Torque screw to 50 IN lbs.
4. Install #1 - #4/0 AWG AL/CU wire and secure wire with wire binding screw. Torque screw to 150 IN lbs.

NOTE: The connector plate, branch lug, wire binding screw and mounting screws are included in the Q1150AN kit. Refer to Instruction Sheet 48040-220-06 (Cedar Rapids).


Revised 4/27/04



CTA-ID : 2009295

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings