Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are QMB Branch Switches 80% or 100% rated devices?
Issue:
QMB continuous current ratings

Product Line:
Panelboards.

Environment:
QMB Switches.

Cause:
Clarification of application of the switch.

Resolution:
The QMB fusible branch switches are restricted to 80% of the current rating of the fuses installed in the switch.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings