Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How much width is required for the EZMCAP closing cap?
Issue:
What is the required width for the EZM closing caps?

Product Line:
US Metering Equipments

Resolution:
EZM main devices are supplied with two closing plates, EZMCAP on the left and EZMSCAP on the right, to cover and seal openings for the horizontal cross bus. The EZMCAP is 2" wide. The EZMSCAP is 1" wide.

When installed in an EZM device, the EZMCAP protrudes 1.8 inches to the left of the enclosure and the EZMSCAP sticks out .77 of an inch to the right.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings