Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number(s) for the 12 inch upper horizontal wireway cover for a Model 6 LVMCC?
Issue:
What are the replacement part numbers for the horizontal wire way, for all widths, at the top of the Model 6 MCC?

Product Line:
Motor control center

Environment:
Model 6

Cause:
Repair parts

Resolution:
The following items are for the upper wireway and not the bottom.
80450-140-50 - 20`` W X 12`` H horizontal wireway cover assembly (includes mounting hardware)
80450-140-51 - 25`` W X 12`` H horizontal wireway cover assembly (includes mounting hardware)
80450-140-52 - 30`` W X 12`` H horizontal wireway cover assembly (includes mounting hardware)
80450-140-53 - 35`` W X 12`` H horizontal wireway cover assembly (includes mounting hardware)




Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings