Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the MP Meter-Pak meter centers suitable for either overhead (top endwall) or underground (bottom endwall) feed applications?
Issue:
Product Design Features

Product Line:
Metering Equipment

Resolution:
All the MP meter center devices are suitable for overhead (top endwall) or underground (bottom endwall) feed applications, but it is up to the installer to obtain local utility approval BEFORE installing any metering equipment.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings