Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does SquareD offer motor circuit protector (magnetic only) breaker for NF panels to be used for motor applications?
Issue:
Is a  motor circuit protector (magnetic only breaker) available  for NF Panels to be used for motor applications?

Product Line:
NF Panelboards and accessories

Environment:
Application/Selection

Resolution:
No we do not offer a motor circuit protector  branch or main for the NF panelboards. NF is primarily used in lighting applications.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings