Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the Current Transformers (CT) offered by SquareD/Schneider Electric rated for use with voltages over 600 volts?

Issue:
Current Transformers are required for Medium Voltage applications

Product Line:
LV Transformers

Environment:
Applies to Current Transformer (CT) products by SquareD/Schneider Electric

Cause:
SquareD/Schneider Electric does not offer Medium Voltage (over 600V) Current Transformers in the North American market

Resolution:

The CTs offered by SquareD/Schneider Electric are not rated for circuits having a phase-to-phase voltage greater than 600 volts.  In certain Medium Voltage applications, additional insulation is applied between the primary and secondary windings to make them serve at higher voltages.   However, SquareD/Schneider Electric assumes no responsibility for damage of equipment or personal injury caused by the Current Transformers operated on circuits above their published ratings.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings