Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What color wires are used for the auxiliary contacts on Square D circuit breakers with a 1212 suffix?
Issue:
Which wire colors apply to which contacts on the 1212 auxiliary contacts?

Product Line:
Legacy Circuit Breakers

Resolution:
The normally open is the yellow wire, the normally closed is the blue wire, and the common is the striped wire.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings