Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does SquareD/Schneider Electric offer fungus proofing of Low Voltage Dry-type Distribution Transformers?
Issue:
Fungus Proofing of Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Dry-type Distribution Transformers by SquareD/Schneider Electric

Cause:
Transformers are sometimes used in high humidity environments


Resolution:
Schneider Electric does not offer fungus proofing for two reasons:
1) the varnish in SquareD/Schneider Electric's Low Voltage Transformers doesn`t promote formation of fungus
2) there is no fungus proofing varnish available that can withstand the standard operating temperature of a Low Voltage Dry-type Distribution Transformer at which point the applied product evaporates.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings