Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the dimensions of the XCM limit switch, such as the XCMA111 limit switch?<br />
See Digest 170, page 17-65.

For this example:

The depth is .63 in
The width is 1.18 in
The height of the body is 1.93 in
The height to the top of the roller is 2.35 in


CTA-ID : 2011365

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings