Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Customer asks if the 8430 MPS is a three phase monitoring device and , if so, why does it only have a SPDT contact?
Issue:
Are the 8430 MPS relays used on 3 phase monitoring?

Product Line:
Relays and Timers

Environment:
8430 Type MPS

Resolution:
Yes. It does monitor all 3 phases. If a single phase, phases reversal, phase unbalance or undervoltage condition is sensed the SPDT contacts change state. (This relays are now obsolete)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings