Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are sensor plugs interchangeable on the Powerpact P and R frame breakers?
Product Line:
Circuit Breakers

Resolution:
Sensor plugs can be replaced only on circuit breakers with date codes later than 07011.

NOTE: This does not apply to ET1.01 trip units. With those trip units, the sensor is fixed and cannot be changed.

Installation Notes:
Sensor plugs are field installable down to 50% of the CURRENT rating. Example: A Powerpact P frame breaker with 800 A sensor installed at the factory can only receive sensors from 400-800 A.  Sensor plugs higher than the original sensor rating cannot be installed.

For complete details on installing sensor plugs and their restrictions, please see the instruction bulletin: 48049-145-03

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings