Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can A.B.Chance ground studs be added to the incoming section of an HVL/cc switch lineup?
Issue:
Adding A.B.Chance ground studs to the incoming section of an HVL/cc switch lineup

Product Line:
HVL/cc Switchgear

Environment:
Installation/Setup

Resolution:
No. A.B.Chance ground studs cannot be added to the incoming section of an HVL/cc switch lineup. The clearances are less than normal in HVL/cc switchgear.

Ground studs would cause internal arcing. An option is to use a main HVL/cc switch with the ground switch option.

Caution must be taken the user must have control of the incoming source.


CTA-ID : 2011924

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings