Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is an EH4, EHB4, EH7 and EHB7?
Issue:
What do the EH4, EHB4, EH7 and EHB7 designations for EH/EHB breakers mean?

Product Line:
Circuit Breakers

Environment:
E frame breakers

Resolution:
EH4/EHB4 is the designation given to 15-60 amp EH/EHB breakers and EH7/EHB7 is the designation given to the 70-100 amp EH/EHB breakers. The 70-100 amp breakers have the rejection feature to prevent breaker installation across from it in the panel.

However, the EH and EHB breakers are all obsolete.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings