Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can AI3 on the Altivar 58 analog I/O (VW3A58201U) card be used as speed reference 2 when using Auto/Manual?
Issue:
AI3 on the ATV58 analog I/O

Product Line:
ATV58

Environment:
All series

Cause:
N/A

Resolution:
No.

The AI3 on the option card VW3A58201U can not be assigned as second speed reference source.
It can only be used as a summing reference to be summed with reference 1.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings