Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What specifications do the double throw safety switches comply with when used for transfer switches?
Issue:
What standards does the Square D double throw safety switches comply with when used for transfer switches?

Product Line:
Safety Switch

Resolution:
The double throw switches comply to UL98 and NEC for transfer switches. It has not been tested to ICS or IEEE standards.
It does not have a molded case switch contact design, so the UL 1008 standard does not apply.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings