Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are separate mounting brackets required to mount a MPZ Mini Power-Zone to a wall?
Issue:
Mini Power Zone Transformer mounting

Product Line:
LV Transformers

Environment:
Applies to Mini Power Zone Transformers from SquareD/Schneider Electric

Cause:
Mini Power Zone Transformers are wall mounted

Resolution:
The MPZ is supplied with the mounting brackets necessary to mount the unit to a vertical structure as designed. It is the installer`s responsibility to provide the appropriate hardware and insure the structure is adequate to support the weight of the MPZ.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings