Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Customer intends to back feed a Transformer. Can the taps be utilized?

Issue:
Using taps on backfed Transformers

Product Line:
LV Transformers

Environment:
Applies to Transformers by SquareD/Schneider Electric

Cause:
Backfeeding on Transformers must be done with recognition of certain limitations

Resolution:

Taps are placed on the primary side of a Transformer to compensate for poor (other than nominal) incoming voltage, allowing the Transformer to operate at it`s designed magnetic flux levels in the core. When backfeeding the Transformer, the magnetic flux level in the core cannot be optimized, since the secondary which is now being fed has no taps to adjust.   When backfeeding, it is best to not use the taps on the primary set at anything but nominal (rated) voltage level.

Schneider Electric USA
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings