Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
In EZM branch devices, are the tenant breakers on the line or load side of the meter socket?
Issue:
Design Features

Product Line:
EZM Metering

Resolution:
The tenant breakers in all EZM branch devices are on the load side of the meter socket. This is known as hot sequence metering as opposed to cold sequence metering, where the breaker would be on the line side of the meter socket (referring to the state of the meter when the breaker is off).

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings