Product Line:
Safety Switches
Resolution:
This kit contains (3) lugs per catalog number. The wiring bending space only allows for (2) #6 - 250 kcmil per phase and neutral. The wire range for the lug is (2) #6 - 300 kcmil. The lugs are mechanical lugs.