Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are most low voltage dry type distribution Transformers offered by SquareD/Schneider Electric rated for 60 Hz, 50 Hz, or 50/60 Hz?

Issue:
Thansformers are available in 50 Hz or 60 Hz configurations, or 50/60 Hz

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Domestic (USA) electrical systems are typically 60 Hz, overseas systems are typically 50 Hz

Resolution:

SquareD/Schneider Electric`s standard offering is 60 Hz rated. SquareD/Schneider Electric can offer Transformers that are rated for 50 Hz or 50/60 Hz (as 50 Hz units can be utilized on either 50 or 60 Hz systems), in which ``50HZ`` is typically part of the catalog number. An exception to that catalog numbering system is the Export Model Transformers shown on page 14-12 of Digest 178 which are 50/60 Hz rated without ``50HZ`` appearing in the catalog number


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings