Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How are the lugs removed from a PowerPacT R frame, I-Line breaker?
Issue:
Removing lugs from a PowerPacT I-Line R-frame breaker

Product Line:
Molded Case Circuit Breakers

Resolution:
The lugs can be removed without taking the breaker apart or removing the protected torx screws. See instruction bulletin number: 48049-256-02

The lugs are to be pried out (gently forced out):
1. With a screwdriver, open the shutter to access and remove lug mounting screws
2. Remove lug with a screwdriver as shown in the instruction bulletin.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings