Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the EZM branch devices without a Lever Bypass on the meter socket(s), be field converted to a meter socket(s) with Lever Bypass?
Issue:
Current Product Design

Product Line:
EZM Metering

Environment:
Product Features

Cause:
Application

Resolution:
NO, the EZM branch devices that do not contain lever bypass on the meter socket(s), CANNOT be field converted to meter sockets with Lever Bypass. The EZM branch devices with the lever bypass will need to be obtained from the factory.

CTA-ID : 2013523

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings