Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the terminal data for a 400 amp main lugs NF panelboard?
Issue:
Terminal data for a 400 amp main lugs NF panelboard

Product Line:
Panelboard

Environment:
NF 400A main lug only panel

Cause:
Product Features

Resolution:
The lugs accept (1)-1/0 to 750kcmil or (2) 1/0 to 350kcmil Al/Cu


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings