Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: Where is the actual catalog number, series number and wiring schematic located on the EZM metering devices?
Issue:
Finding the catalog & series number and wiring schematic on EZ Meter-Pak Meter Center main or branch devices.

Product Line:
EZ Metering

Resolution:
The actual catalog and series number, along with the wiring schematic and other general information about the EZM Main Devices, will be located on the Wiring Diagram Label, which is located on the back side of the Front cover.

The actual catalog and series number, along with the wiring schematic and other general information about the EZM Branch Devices, will be located on the Wiring Diagram Label, which is located on the back side of the Tenant Breaker Compartment cover (or the customer compartment cover).

NOTE: To Actually see the wiring diagram label, it requires the front covers to be REMOVED from the Main device and the Tenant breaker cover(or customer cover) to be REMOVED from the branch device.

SEE BELOW A VISUAL OF A MAIN DEVICE AND BRANCH DEVICE WIRING DIAGRAM LABELS. ALSO SEE BELOW A VIDEO.

THE BELOW LABELS ARE ONLY SAMPLE LABELS, THE LABEL THAT COMES ON THE PARTICULAR DEVICE WILL CONTAIN INFORMATION SPECIFIC TO THAT DEVICE.
Image of a label as an example

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings