Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: The 9013 GHG2J99X 2-way pressure valve always leaks air causing the compressor to cycle on and off.
Look to see if there is a check valve in the system. The check valve should only allow air to flow in one direction. If the check valve is stuck open or missing then all of the air in the line will drain back through the 2 way valve causing the compressor to kick back in.

Note: The check valve is a user supplied part and is not part of the 9013 pressure switch.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings