Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H222AWK, series F6 (F06) safety switch?
Issue:
What replacement parts are available for the H222AWK, series F06?

Product Line:
Safety Switches

Resolution:
The replacement parts for the H222AWK, series F6 (F06) are as follows. No other parts are available.
Line Base Assembly - 4056642150 (1 required; arc suppressor assembly and fuse puller not included)
Load Base Assembly - 4056002650 (1 required)
Arc Suppressor Assembly - 4056001801 (1 required)
Fuse Puller Kit - FPK03
Lug Assembly - 4025101652 (per lug)
Switch Mechanism - 4056610750 (also recommend replacing switch mechanism gasket)
Switch Mechanism Gasket - 4056665601
Handle Assembly - 4056684150K
Handle Gasket - 4056603101
Lockplate - 4056637601
Line & Load base mounting screw - 4020516001 (3 for line and 2 for load)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)
Handle Gasket - 4056603101
Lockplate - 4056637601
Line & Load base mounting screw - 4020516001 (3 for line and 2 for load)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)
Equipment Ground Lug Kit - GTK03

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings