Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the replacement parts for the H321A, series F6? (may be shown as F06)
Issue:
What are the replacement parts for the H321A, series F6? (may be shown as F06)

Product Line:
Heavy Duty Safety Switch

Environment:
Replacement parts

Cause:
Maintenance required

Resolution:
The replacement parts for the H321A, series F6 (F06) are as follows. No other parts are available.

Line Base Assembly -4056642450 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 4056641150 (requires one per switch)
Arc Suppressor Assembly - 4056001801 (requires one per switch)
Fuse Puller - FPK03
Lug Assembly - 4025101652 (per lug)
Switch Mechanism - 4056610750
Switch Mechanism Gasket - 4056665601
Handle Assembly - 4056684150K
Handle Gasket - 4056603101
Lockplate - 4056637601
Line & Load base mounting screw - 4020516001 (3 for line & 2 for load)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)
Equipment Ground Lug Kit - GTK03

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings