Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the maximum fuse ampere rating that can be used in a factory or field installed fuse block or fuse clip for a 9070 Type T or TF Industrial Control Transformer?
Issue:
Fuse ampere rating

Product Line:
LV Transformers

Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric

Cause:
Fuseholders  for Type T and TF Industrial Control Transformers


Resolution:

The maximum ampere rating of the fuse blocks and fuse clips offered by SquareD/Schneider Electric for the 9070 Type T and TF Industrial Control Transformers is 30 amps.  If higher fuse ratings are required, then the customer will have to provide the suppplementary fuse holder provisions.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings