Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H364A, series F6? (may be shown as F06)
Issue:
The list of repair parts is needed for Safety Switch catalog number H364A, series F6.

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the H364A, series F6 (F06) are as follows. No other parts are available.
-Line Base Assembly - 4056703450 (1 required - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line Base mounting screws - 4020546401 (2 required per line base)
-Load Base Assembly - 4056677450 (1 required per phase - includes phynolic base, lugs, and fuse clips)
-Load Base mounting screws - 4020546401 (2 required per load base)
-Arc Suppressor Assembly - 4056677550 (1 required per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Mounting Screw - 2140122240
-Switch Mechanism - 4056678650 (also requires switch mechanism gasket 4056786001)
-Switch Mechanism mounting screws- 2299940562 (2 required)
-Handle Assembly - 4056663550 (also requires handle gasket 4056603101)
-Lockplate - 4056672101
-Lockplate mounting screws - 2299940562 (2 required)
-Equipment Ground Lug Kit - PKOGTA2

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings