Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the dimensions of the standard circuit directory card for NQOD and NF panelboards catalog number 80031-158-01?
Issue:
Dimensions of the standard circuit directory card for NQOD and NF panelboards catalog number 80031-158-01

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The card is approx. 5 1/2`` X 5 1/2`` square.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings