Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What type of hub is used with an OCK400 overhead trough?
Issue:
Selection

Product Line:
CSED

Resolution:
The top endwall is provided with a hub opening, accepting a field installed "A-L" type of hub. A-L type hubs are available for 2" thru 4" conduit.
2" = A200L
2.5" = A250L
3" = A300L
3.5" = A350L
4" = A400L
There is a concentric knockout pattern in the lower, right side wall for user supplied conduit to route the conductors into the CSED device. The knockout pattern is for 2.5", 3", 3.5" and 4" generic conduit hubs.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings