Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What CSED catalog numbers can the overhead trough, part number OCK400, be used with?

Issue:
Product design features

Product Line:
Combination Service Entrance Devices

Resolution:
The OCK400 is listed as an accessory on the wiring diagram of the following 400 A CSEDs:

P/N#P/N#
CU12L400CB RU2040D400PCL
CU12L400CN RU2040D400PCLX
CU816D400CN RU3040D400CK
CU816D400PCN RU3040D400CL
QU12L400CL RU3040D400CLX
QU12L400SL SU2040D300PCN
QU816D400CL SU2040D400PCB
QU816D400CLX SU2040D400PCN
QU816D400PCL SU3040D300CN
QU816D400PCLX SU3040D400CB
QU816D400PSLSU3040D400CN
QU816D400SL


NOTE: This trough DOES NOT allow for entering the top endwall on any of the 400 A CSED devices. As shown below, it is ONLY a trough for routing the service wires into the top of the trough, then down through the trough to enter the CSED devices from the bottom.
Trough drawing
Installation instructions;
Instructions



Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings