Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the replacement parts for the H364NA, series F6? (may be shown as F06)
Product Line:
Heavy Duty Safety Switch

Environment:
Applicable only to H364NA, series F6.

Resolution:
-Complete Line Base - 4056703450 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line Base mounting screws - 40205-464-01 (requires 6 per line base)
-Load Base Assembly - 40566-774-50 (requires one per phase - includes phynolic base, lugs and fuse clips)
-Load Base mounting screws - 40205-464-01 (requires 2 per load base)
-Arc Suppressor Assembly - 40566-775-50 (requires one per phase)
-Arc Suppressor mounting screw - 40205-145-01
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 21401-222-40 (per lug)
-Switch Mechanism - 40566-786-50 (also requires Interlock Shaft Gasket 40567-860-01)
-Switch Mechanism mounting screws- 22999-405-62 (requires 2)
-Handle Assembly - 40566-635-50 (requires handle gasket 40566-031-01)
-Lockplate - 40566-721-01
-Lockplate mounting screws - 22999-405-62 (requires 2)
-Neutral Assembly - SN20A
-Neutral Bonding Screw - 40283-566-51

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings