Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is Short Time Current, 2 sec. rating for the HVL switch?
Issue:
Short time for a MV HVL switch

Product Line:
MV switch

Environment:
HVL

Resolution:
Short Time Current is the maximum current a switch/device can carry for 2 seconds without damage to the switch/device. Short time current is the only one of these three that is expressed in symmetrical amperes. Momentary and Fault Close currents are expressed in Asymmetrical amperes. ASYM Amps = 1.6 X SYM Amps.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings